SDP/SI Home Page
Free Catalogs
acme lead screws, small parts, timing belts, couplings,shafts
Corner2.gif (1203 bytes)

main_logo2.gif (2264 bytes)

logo_newblack.GIF (11050 bytes)
right_white.GIF (957 bytes)
SDP/SI Company Profile
Sales Reps.
New Products

       New Shafts & Accessories

DWG DrawingsFree VideoRelated CompaniesTechno-IselTechno-Sommer Home Page

New Series Of Grip Fast™ Quick Release Shaft Collars From SDP Can Be Removed Or Adjusted in Seconds

Image Driven Product Finder & Current Prices 

A new series of Grip Fast™ quick release shaft collars from Stock Drive Products (an ISO 9001 manufacturer) are self-locking, quick release collars that can be removed or adjusted in seconds using only one hand, without tools. Applications for this patented system are numerous, and include: fastening rotating components, and as a limit stop for 23 shaft sizes ranging from 1/8" up to 3".

Identified as the A 7Z34 Series, they absorb vibration and shock, lower downtime, and maximize production time. To operate: 1-simply slide Grip Fast™ onto the shaft to the correct location. 2-It will automatically lock into position. 3-To release, simply push Grip Fast™ slightly forward. Then squeeze between the end ring and outer body gap (to cause the gap to become wider). Then slide Grip Fast™ off. Availability is from stock in both inch and metric sizes.

Here is how they work. There are six basic components. The inner mechanism is comprised of three steel balls, one retention ring with a tapering inner diameter, and one spring. The ABS composite housing consists of one inner body, an outer sleeve, and an end release ring. The inner body is drilled to accommodate the three balls so that they emerge through its inner diameter. They rest against the tapered retention ring. This causes the ball bearings to squeeze down on the cylindrical shaft with the same size OD as the inner body's bore, jamming the ball bearing between the shaft and the retention ring. This locks the Grip Fast™ (and any object it is set up against) in the opposite direction. An undercut between the retention ring and outer sleeve gives the ring more flexibility, which under unsymmetric loading, causes more uniform distribution of the forces in the balls. The housing parts hold all of this together and are spring-loaded. To release the Grip Fast™, the inner body is pulled back through the inside of the outer sleeve, pulling the ball bearings out of the gap between the inner body and the shaft, and releasing the collar's hold on the shaft. The spring forces the inner body back to the closed position. The distance that exists between the end release ring and the outer sleeve is designed to allow one handed release.

Detailed technical specifications for inch sizes are contained in Catalog D790, available free upon request from Stock Drive Products, 2101 Jericho Turnpike, P.O. Box 5416, New Hyde Park, New York 11042-5416. Phone: 516-328-3300 • Fax: 516-326-8827. 
Web: http://www.sdp-si.com  

SDP2  27

red_blank.gif (895 bytes)

Top of Page

| Home | Free Catalogs | Company Profile | Sales Reps. |
New ProductsVideo | Recent Ads |
 Techno-Isel  | Techno-Sommer |

Stock Drive Products / Sterling Instrument
E-Mail: SDP-SIsupport@sdp-si.com
Phone: 516-328-3300
Fax: 800-737-7436 or 516-326-8827

 

 

bottom_line.gif (80 bytes)