![]() ![]() |
New Series Of Hydro-Dynamic Pressure Bearings From Sterling Instrument Feature Unique Construction Image Driven Product Finder & Current Prices
grease containing antioxidant and anticorrosion additives. The inner faces of these laminated plates act as the bore of the assembled bearing. When the shaft rotates in this state, a fluid between the shaft guide and the shaft generates pressure as a result of the "squeeze effect" - a phenomenon of generating pressure to a lubricating membrane in a fluid lubrication when wall faces are close to each other. The 7 bearings in the
series have I.D.'s ranging from 1 to 6 mm and an impressive maximum speed
range of from 6000 to 20000 rpm. |
|
| Home
| Free Catalogs | Company Profile | Sales
Reps. | Stock
Drive Products / Sterling Instrument
|